Does the IPU_CSI0_SENS_CONF[CSI0_SENS_PRTCL] need to be set? Does it refer to the MIPI Clock coming from the camera. For instance, the OV5675 can be programmed to gate the MCP/MCN when no data is transmitted. Of does this refer to some internal signal?
Is this accurate for Bayer 10-bit,
1920x1080 (pixels/frame) x 10 (bits/pixel) / 8 (bits/cycle) x30 (frames/second) x 1.35 = 105 MHz;
I can't seem to force an EOF - does anyone have any ideas why that might be?
My [mostly] complete configuration is described here.
Why oh why is this marked assumed answered!?!?1
Hi Nate
MIPI usage is described in AN5305 MIPI–CSI2 Peripheral on i.MX6 MPUs
https://www.nxp.com/docs/en/application-note/AN5305.pdf
MIPI CSI2 data transferred from MIPI CSI to IPU Gasket to IPU CSI and it is always
in non-gated clock mode. Bayer example can be found on
i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------