iMX6DL can mirroring the LVDS and VGA(external monitor)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL can mirroring the LVDS and VGA(external monitor)?

705 Views
호영노
Contributor II

I'm using the iMX6DL and linux 3.0.35 kernel.

One display connected to the LVDS output of the iMX6DL and the VGA Moniotr is using the external analog devices ADV7125 DAC. 

As I reviewed so many threads in this community which concerned about mirroring.

At this time, I could see the each output but I couldn't see the mirroring output. (same time, same screeen)

If I want to mirroring of LVDS and LCD, then it need 2 IPU?

Because iMX6DL has only 1 of IPU,

so I set the same IPU id to LVDS and LCD. 

And I set the different channel of disp_id.

But it doesn't working.

here is my uboot code

"root=/dev/mmcblk0p1 rootfstype=ext4 rootwait rw video=mxcfb0:dev=ldb,LDB-VGA, ldb=sin0 bpp=32 video=mxcfb2:dev=lcd, LCD-640480, bpp=32, if=RGB24\0"

I set the mxcfb0 to ldb, and mxcfb2 to LCD.

this is LDB's timing 


{
"LDB-VGA", 60, 640, 480, 15385,
100, 40,
30, 3,
10, 2,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},
};

And LCD's timing is 

{
"LCD-640480", 60, 640, 480, 39683, 45, 114, 33, 11, 1, 1,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},

when I check the fbset in terminal,

fb0 and fb2 is same as LDB-VGA's timing.

It seems like my uboot code is not working. (mxcfb2's setting.)

Because if I change the mxcfb0 to lcd and mxcfb2 to lvds, 

then lcd is working but lvds is not working.

What can I do? 

Is this need to 2 of IPU?

Labels (2)
Tags (2)
0 Kudos
1 Reply

559 Views
igorpadykov
NXP Employee
NXP Employee

Hi 호영 노 

may be useful to check

Screen mirroring on VAR-SOM-MX6 - Variscite Forums 

in general 1 IPU should be sufficient, for example on below link

ipu_id = 0 used for both lcds:

Can I mirror a LVDS channel on HDMI? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos