Question, i.MX28 24MHz crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX28 24MHz crystal

752 Views
SLICE
Contributor IV

Dear team,

My customer is using i.MX28 for their board now, and they want to change 24MHz crystal from the current one.
Could you show me whether there is a specification on i.MX28 about the period from start of oscillation to its stabilization?

Thanks,

Miyamoto

Labels (1)
0 Kudos
3 Replies

531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

I am afraid i.MX28 crystal start-up time specs are not available.

One can follow design check list and crystal requirements on

Hardware Design Checklist for i.MX28 

In general time to crystal stabilization is defined by crystal Q factor

(typical Q value for a quartz oscillator ranges from 10**4 to 10**6),

it requires (roughly) Q number periods until crystal become stable.

Crystal oscillator - Wikipedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

531 Views
SLICE
Contributor IV

Hi igorpadykov

Thanks for your support.

They believes that i.MX will do switching clock or releasing reset internally after stabling the oscillation.

Can I understand that users do not have to detect the stability of the oscillation externally?

Best Regards,

Miyamoto

0 Kudos

531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes this is correct understanding.

Best regards
igor

0 Kudos