SiI1127A to i.MX7D CSI Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SiI1127A to i.MX7D CSI Interface

Jump to solution
729 Views
ko-hey
Senior Contributor II

Hi all

 

Does someone have experience for connecting Sli1127A and i.MX7D CSI ?

 

I am trying to interface Sil1127A hdmi chip with IMX7 processor

So I want to confirm the signal connections.

 

Here is a connection what I think. Does it correct ?

 

DE                      

HSYNC                CSI_HSYNC

VSYNC                           CSI_VSYNC

ODCK                            CSI_PIXCLK

Q                                   CSI_DATAxx

 

 

I also refer to the following thread and DE signal don't need to connect.

https://community.nxp.com/message/881323

 

Here is a datasheet for Sil1127A.

http://www.latticesemi.com/-/media/LatticeSemi/Documents/DataSheets/ASSP/SiI-DS-1059_Public.ashx?doc...

 

add info:

I'll not use audio data in my system.

 

 

BR,

Kohei Tanaka

 

0 Kudos
1 Solution
498 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kohei 

connections seem as correct, you are right DE signal is not needed.

Best regards
igor
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
499 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kohei 

connections seem as correct, you are right DE signal is not needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos