QN9083 IEEE address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9083 IEEE address

448 Views
waynejeong
Contributor II

Hello.

We are considering BLE product using QN9083 for mass production.

If the product will be mass production, do we need to write BD address in rom or flash memory? or is there included unique BD address in rom or flash?

Thank you.

0 Kudos
1 Reply

339 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Wayne Jeong,

The QN908x have an unique Bluetooth address stored in flash. See 7.3.1.1 Flash information page in the QN908x user manual

There is also a special area in the flash called Non-Volatile Data Storage (NVDS), which is used for user information and can contain a custom Bluetooth address, the BLE stack will try to load the address from the NVDS first and if it is not present it will use the default Bluetooth address from the Flash information page.

Let me know if you have any question.

Regards,

Gerardo

0 Kudos