Skip navigation
Log in to follow, share, and participate in this socialgroup.

Recent Activity

Jeremy Geslin
Click to view contentCombining NXP's wireless MCU with NFC controller allows to build a BLE-NFC bridge. It allows demonstrating transmission of NFC data over BLE, acting then as a king of Magic NFC remote.   This demonstrator is built assembling the OM5578: Development Kits for PN7150 Plug’n Play NFC Controller (OM5578/PN7150ARD version including Arduino compatible…
in DemoLab
Iain Galloway
Click to view contentQGroundControl mission planner optimized by Qt Company to run on a Technexion TEP-15 industrial panel computer. QGroundControl is part of the Dronecode Platform.   ======= Please see www.hovergames.com and www.nxp.com/hovergamesdrones for more drone hardware. =======   Features: A low power, rugged, fan-less, cost effective reference solution…
in DemoLab
Jeremy Geslin
Click to view contentThis document describes step-by-step how to run NFC on Raspberry Pi platform.  Hardware setup:You need:    - Raspberry Pi (any model except Pi zero) : https://www.raspberrypi.org/products/:                                                        - OM5578(PN7150 demokit) in RPi configuration (or OM5577(PN7120 demokit)):         Then simply…
in DemoLab
Lauren Percy
Click to view contentThe demo shows the NXP Beacon implementation running on Kinetis KW40 Wireless SoC.  At the start-up the FRDM-KW40Z board starts sending advertisements packets each ~2 seconds and the BLE beacons are captured from the NXP Smartphone app that implements Bluetooth Beacons profile.  A Beacon is a non-connectable device that uses Bluetooth Smart…
in DemoLab
edk
Demo The MC33SB040X familly is an antilock brake controller designed especially for two wheeler system. Thanks to the plug and play evaluation module controlled by a friendly graphical unit interface, we will show the potential of our product.  Through this demo, we will demonstrate how it is easy to use our solutions and accelerate the…
in DemoLab
edk
Demo Wheel rotation is controlled by the SB0400 DC motor pre-driver. When the wheel is stopped manually, the Wheel Speed Sensor -KMI23- detects it & sends a signal to the SB0400 motor pre-driver & S32K MCU to activate the electromagnet   Products 32-bit Automotive General Purpose MCUs|NXP Motorcycle Two-Wheel Antilock Braking (ABS)|NXP…
in DemoLab
edk
Click to view contentExplore the MC34937, an industrial-grade 3-phase gate pre-driver for BLDC and PMSM motor control. The MC34937 can support 12V, 24V, and 36V motor control applications and easily interfaces to standard MCUs and DSPs. The demo shows the implementation of the MC34937 with Kinetis Microcontrollers E in a 36V battery-operated electric bike (eBike)…
in DemoLab
Marcin Jurczyński
Low power Eink or ePaper is all about low power, just like MpicoSys. To enable best use power-wise we have over the years developed multiple timing controllers for various displays. With the introduction of the 9.7” we now have a complete product family for E Ink displays. And with an impressive power performance. Update in below zero temperatures… (Show more)
in DemoLab