Q&A: What is the value on NVCC_LVDS_2P5?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Q&A: What is the value on NVCC_LVDS_2P5?

Q&A: What is the value on NVCC_LVDS_2P5?

Question:

What does it means by depending on load? Is there a value?

image001.png

This is  related with i.MX6D

Answer:

The comment about the "load" means the total system load on the 2.5V rail. We understand that people design systems, not just MX6 devices. The documentation confusion stems from the design team changing from allowing customers to use the LDOs to power system devices back to just using the LDOs to power the MX6. Reasons - thermals, and also concern for uncontrolled system noise injection into the MX6 and causing failures.

Labels (1)
Tags (2)
No ratings
Version history
Last update:
‎10-09-2013 11:48 PM
Updated by: