Formula SAE Electric Vehicles USA 2013 winner is the Brazilian team from UNICAMP
Formula SAE Electric Vehicles USA 2013 winner is the Brazilian team from UNICAMP
This past Tuesday June 25th, 2013, the UNICAMP E-Racing compete against 19 teams and won the first place with a score of 985 points of a total of 1000.
The car used an electric motor of 120 V and a chassis that weighted 250 kg (551.2 lbs). That allows the car with a charging time of 2 hours to be driving for 25 km (15.5 miles) and race up to speeds of 170 km/h (105.6 mph).