CodeWarrior+Kinetis Reference Manual.

Document created by Monica Arvizu Employee on Oct 16, 2012Last modified by Diana Torres on Feb 28, 2017
Version 2Show Document
  • View in full screen mode

Even though there has been a huge rush to get the latest versions of CodeWarrior for MCU, I've also got some questions regarding the compiler and linker version 10.0, so I'll share with you the Kinetis Refernce Manual for MCU v10.x


The Kinetis (also known as ARM or Cortex-M4) Build Tools Reference Manual for Microcontrollers describes the compiler used for the Freescale 32-bit Microcontroller Unit (MCU) chip series.


This application note provides information about the CodeWarrior compiler and its linker, versions 10.0 and higher and explains how to use CodeWarrior tools to build programs.


CodeWarrior build tools translate source code into object code then organize that object code to create a program that is ready to execute. CodeWarrior build tools run on the host system to generate software that runs on the target system. Sometimes the host and target are the same system. Usually, these systems are different.


The document also provides information about the documentation related to the CodeWarrior Development Studio for Microcontrollers, Version 10.x and contains these major sections:

• Compiler Architecture

• Linker Architecture

• Additional Information Resources

• Miscellaneous


Ready to give it a glance?  Do it now!

Kinetis Build Tools Reference Manual Kinetis Build Tools Reference Manual