Have additional flash devices? Use them!

Document created by Monica Arvizu Employee on Sep 9, 2012Last modified by Diana Torres on Feb 28, 2017
Version 2Show Document
  • View in full screen mode

This document explains how to use the Flash Tool Kit to support additional flash devices on the Flash Programmer for CodeWarrior Development Studio for Microcontrollers V10.0 by creating new programming algorithms and support files.


This application note applies only to the external flash devices used with ColdFire V2/V3/V4 processors.



This document includes these topics.


• Create a flash device XML configuration file

• Create new target task

• Create external flash algorithm

• Flash programmer examples

• Create new flash utility

• Flash utility examples

• Troubleshooting flash programmer


The application note we are here suggesting provides you the necessary info to add devices to the FreescaleCodeWarrior Flash Programmer, along with some specifications that might be really useful depending on each CPU setup and the files and documentation that is required.


Many manufacturers use the same flash device algorithms, so it is likely that flashes can be programmed using the algorithms included with the CodeWarrior software. In addition, many manufacturers produce devices compatible with those of Intel, Advanced Micro Devices (AMD), or STMicroelectronics (ST).


Anyways, enjoy and keep finding interesting content with DebuggerGuys!


Adding Device(s) to CodeWarrior Flash Programmer for Microcontrollers V10.0