FreeRTOS_1.199_18.08.2012.PEupd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS_1.199_18.08.2012.PEupd

FreeRTOS_1.199_18.08.2012.PEupd

FreeRTOS

DescriptionFreeRTOS (www.freertos.org) implementation as component. Support for all S08 and all S12(X), ColdFire V1 (CN, JM, QE, JE, and MM families), ColdFire V2 (5225x) and all Kinetis (tested with K40, K60, K70/M4F, KL20Z Freedom Board).
ComponentFreeRTOS.PEupd
DependenciesUtility, FreeRTOSTrace, PercepioTrace

A tutorial how to use the FreeRTOS Embedded Processor Expert component is used can be found here: Tutorial: FreeRTOS on DEMOJM

Attention Classic (non-eclipse) Users!

The component has been tested with CodeWarrior for S12(X) V5.1, which is not eclipse based. The eclipse based CodeWarrior (MCU10.x) is using the concept of an RTOS adapter. The FreeRTOS component has now a setting to disable this. You need to set the setting 'Classic CodeWarrior' to 'yes' in order to have it working in a non-eclipse CodeWarrior environment. Otherwise you will see internal errors during code generation.

Additionally at least the PE 3.09 Service pack needs to be installed. The update is available on http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63, direct link:CodeWarrior for MCU V6.3 Processor Expert V3.09 Update

RTOS adapter settings for classic CodeWarrior

License

License : Open Source (LGPL)
FreeRTOS (c) Copyright 2003-2012 Richard Barry, http: www.FreeRTOS.org
FreeRTOS Processor Expert Component: (c) Copyright Erich Styger, 2012
Processor Expert and CodeWarrior (c) Copyright Freescale Semiconductor, 2012, all rights reserved
This is a free software and is opened for education, research and commercial developments under license policy of following terms:
* This is a free software and there is NO WARRANTY.
* No restriction on use. You can use, modify and redistribute it for personal, non-profit or commercial product UNDER YOUR RESPONSIBILITY.
* Redistributions of source code must retain the above copyright notice.

Labels (1)
Attachments
No ratings
Version history
Last update:
‎09-09-2012 11:51 AM
Updated by: