RD56F8300FRBBW: FlexRay Brake-By-Wire Reference Design using 56F8300 DSCs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RD56F8300FRBBW: FlexRay Brake-By-Wire Reference Design using 56F8300 DSCs

RD56F8300FRBBW: FlexRay Brake-By-Wire Reference Design using 56F8300 DSCs

Overview

The FlexRay Brake-By-Wire reference design shows FlexRay capabilities such as high communication speed and channel fault detection.

  • It uses the NXP® MC9S12XDP512 MCU for the pedal node and MC56F8346 DSC for the brake/wheel node; FlexRay connectivity of both nodes is based on the MFR4200 FlexRay communication controller
  • The braking caliper is controlled by PMSM using Vector Control technique while the spinning wheel representing a real tire is powered by a BLDC motor
  • The boards of the 2 engines are interconnected by a CAN bus
  • Uses FlexRay baud rate of 10Mb/s per channel but both channels carry the same data, which enables demonstration of the FlexRay channel fault detection feature

Features

  • PMSM using Vector Control technique
  • FlexRay communication speed 10Mb/s per channel
  • Dual channel connection
  • Channel fault detection
  • Re-connection feature
  • FreeMASTER tool based control pages

Block Diagram

RD56F8300FRBBWBLK.gif

Board

RD56F8300FRBBWIMG.jpg

Design Resources

Labels (1)
Attachments
No ratings
Version history
Last update:
‎08-11-2020 06:00 PM
Updated by: