Compile the sample project within MCAL, like S32K14X_MCAL4_2_RTM_1_0_0

Document created by Oliver Tian Employee on Jul 30, 2020
Version 1Show Document
  • View in full screen mode

Hi, 

   If you try to compile the sample project within S32K14X_MCAL4_2_RTM_1_0_0, you should take care of the command if you use Linaro.

   After you set the environment of compiling and run the command under command window, you should enter 

   "launch.bat MODE=USER TOOLCHAIN=linaro"

 

   NOT

   "launch.bat MODE=USER TOOLCHAIN=LINARO"

 

   The command is case sensitivity.  

 

Hope you can compile the project successfully. 

 

Cheers!

Oliver

Attachments

    Outcomes