i.MX RT600 Audio Playback GUI Demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT600 Audio Playback GUI Demo

i.MX RT600 Audio Playback GUI Demo

Overview

   This demo uses the i.MX RT600 EVK (MIMXRT685-EVK) with a GUI software to playback MP3 files. An equalizer can be switch on to demonstrate the HiGi-4 audio DSP. Beside the board itself it requires a SD-card with MP3 music tracks and a portable speaker or headphone.

   The i.MX RT600 is a crossover MCU family optimized for 32-bit immersive audio playback and voice user interface applications combining a high-performance Cadence® Tensilica® HiFi 4 audio DSP core with a next-generation Cortex-M33 core. The i.MX RT600 family of crossover MCUs is designed to unlock the potential of voice-assisted end nodes with a secure, power-optimized embedded processor.

Demoing Guide

No software installation required to demo this board. To build this demo, pls. refer to the description at the end of this guide.

  • Insert the SD-Card with mp3 files to on-board SD Card connector, not to the one below the LCD board
  • Connect headphones or external speakers to the 3.5mm jack Line Out (J4)
  • Supply the board through Micro-USB connector (J5) in the upper right edge

Three main windows/tabs on the GUI:
File playback
This screen shows:
• Album artwork/NXP logo
• Current track information (title, artist, album)
• Media controls (prev, play/stop, next)
• Volume slider

pastedImage_8.png

Playlist
This screen shows:
• Playlist information from mp3 files found in SD card
• A track for playback can be selected by touching the line

pastedImage_9.png

Spectrum visualizer
This screen shows:
• Seven vertical bars showing the frequency spectrum of the current track being played.
• Button for toggling Equalizer On/Off
o if on the sound is AM radio style

pastedImage_10.png

Products

i.MX RT600 Evaluation Kit | NXP 

Labels (1)
Attachments
No ratings
Version history
Last update:
‎07-19-2020 07:59 PM
Updated by: