Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

Application Note (AN12765): DSP Enablement for i.MX RT600 MCUs - XOS Use Cases

The i.MX RT600 MCU includes a Cadence® Tensilica® HiFi 4 DSP running at frequencies of up to 600 MHz.The XOS embedded kernel from Cadence is designed for efficient operation on embedded system built using the Xtensa architecture. Although various parts of XOS continue to be tuned for efficient performance on the Xtensa hardware, most of the code is written in standard C and is not Xtensa-specific.

Click here to access the full application note.

Labels (1)
No ratings
Version history
Last update:
‎03-05-2020 12:55 PM
Updated by: