Overview
In this demo we show how to load an example of an NFC reader using the combination between the UDOO NEO card and the development kit for the PN7150.
PN7150ARD kit is a high performance fully NFC compliant expansion board compatible with Arduino Compatible Interface platforms. It meets compliance with Reader mode, P2P mode and Card emulation mode standards. The board features an integrated high-performance RF antenna to insure high interoperability level with NFC devices.
Video
Required Items
- UDOO NEO
- Compatible MicroSD card of at least 4 or 8 Gb memory size
- Micro USB cable
- UDOO Neo demo image file
- PN7150 NFC Controller Board
Links
Step by Step guide (Inlclude all links): https://www.nxp.com/docs/en/application-note/AN11841.pdf