aips_demo_s32k118.zip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

aips_demo_s32k118.zip

aips_demo_s32k118.zip

Example of usage of AIPS-lite, Protects the access to GPIO port. This example can be used with UART terminal, 115200 bps. The interface menu shows like this:

AIPS example has started
Please press 0 + enter to set red LED in GPIO port
Please press 1 + enter to set red LED in GPIO port
Please press 2: GPIO peripheral will only accept accesses from trusted master, M0 (Core) is set as untrusted when a write access, AIPS cannot longer be modified from core and a reset will occur in the next GPIO access
Please press 3: GPIO access is write protected, any write access to GPIO will produce a hard fault

Attachments
No ratings
Version history
Last update:
‎09-25-2019 01:25 AM
Updated by: