Update firmware and Erase and re-program a FRDM-KV31F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update firmware and Erase and re-program a FRDM-KV31F

Update firmware and Erase and re-program a FRDM-KV31F

I have included the files needed to mass erase the flash of the MCU and re-program another binary.  

The procedure is shown in the folder " FRDM-KW31_FAT_added_2019"

Summarizing you...

1) update the debugger with bootloader mode (press reset and plug in usb cable) drag and drop .sda file on MSD bootloader.

2) unplug and re-plug USB. program the flashloader_loader_mkv31f512.bin by dragging and dropping the binary on to the virtual mass storage device FRDM-KV31 which appear when you plug the USB cable from the FRDM-KV31 to the PC. 

3) Open a CMD prompt window and navigate to the folder the files were unzipped to.

4) Determine the COM port by using the device manager

5) from the CMD prompt run the batch file 
    Erase_KMS_program_bubble.bat COMX

Attachments
No ratings
Version history
Last update:
‎09-03-2019 02:36 PM
Updated by: