S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed.
Prerequisite
Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS.
1) Launch S32DS
2) Select 'New S32DS Project from example'
3) Select apex2_fast9 project
4) Click Finish
5) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'.
6) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9.
7) Click Resume