Target request fail : GDI protocol Adapter: stop failed,Non Fatal Error

Document created by Junjie Lai Employee on Feb 19, 2019
Version 1Show Document
  • View in full screen mode

Sometimes we don't use external debugger but OpenSDA on-board . The debugger controller clock setting need more attention because of slow debug by OpenSDA on-board. if you set the bus clock too high to make step by OpenSDA. The Non error will report at the stage of download(Fig2) and pause, even stop(Fig1).

Fig 1  Pause and stop error 

Fig 1  Download error 

when you encounter. you can set debugger follow some steps.

1 open debug configurations-Target setting-Edit...

2 In Edit you need remove the selection of 'use bus clock as debug controller clock source ' and then reopen the CW and project debug fine works.

 

Enjoy!

Attachments

    Outcomes