Yocto BSP compile ERROR

Document created by Jackson Williams on Jan 24, 2018
Version 1Show Document
  • View in full screen mode
$MACHINE=pico-imx7 BASEBOARD=pi source edm-setup-release.sh -b build-fb-pico-imx7 -e fb $bitbake fsl-image-qt5

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "pico-imx7"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.1.0"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser = "HEAD:393d2aa15da21ffa532c3cd77d8cb91de997cd31"
meta-gnome
meta-networking
meta-python
meta-ruby
meta-filesystems
meta-xfce = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"
meta-edm-bsp-release = "HEAD:5fc6577b217cf0c172391e0635dec2cfe146e155"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: perl-native-5.22.1-r0 do_fetch: Failed to fetch URL http://www.cpan.org/src/5.0/perl-5.22.1.tar.xz, attempting MIRRORS if available
WARNING: mesa-2_11.1.1-r0 do_fetch: Failed to fetch URL ftp://ftp.freedesktop.org/pub/mesa/11.1.1/mesa-11.1.1.tar.xz, attempting MIRRORS if available
WARNING: python-setuptools-19.4-r0 do_fetch: Failed to fetch URL http://pypi.python.org/packages/source/s/setuptools/setuptools-19.4.tar.gz, attempting MIRRORS if available
WARNING: imx-vpu-1_5.4.35-r0 do_fetch: Checksum mismatch for local file /home/user/workspace/edm_yocto/downloads/imx-vpu-5.4.35.bin
Cleaning and trying again.
WARNING: imx-vpu-1_5.4.35-r0 do_fetch: Renaming /home/user/workspace/edm_yocto/downloads/imx-vpu-5.4.35.bin to /home/user/workspace/edm_yocto/downloads/imx-vpu-5.4.35.bin_bad-checksum_afe1edb51832de0cfec0b67b4779b231
WARNING: imx-vpu-1_5.4.35-r0 do_fetch: Checksum failure encountered with download of http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-5.4.35.bin;fsl-eula=true - will attempt other sources if available
WARNING: imx-codec-4.1.6-r0 do_fetch: Checksum mismatch for local file /home/user/workspace/edm_yocto/downloads/imx-codec-4.1.6.bin
Cleaning and trying again.
WARNING: imx-codec-4.1.6-r0 do_fetch: Renaming /home/user/workspace/edm_yocto/downloads/imx-codec-4.1.6.bin to /home/user/workspace/edm_yocto/downloads/imx-codec-4.1.6.bin_bad-checksum_9b4cf958d86941ee35eab9ff90acb2e5
WARNING: imx-codec-4.1.6-r0 do_fetch: Checksum failure encountered with download of http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-codec-4.1.6.bin;fsl-eula=true - will attempt other sources if available
ERROR: imx-codec-4.1.6-r0 do_fetch: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-codec-4.1.6.bin;fsl-eula=true'. Checksum mismatch!
File: '/home/user/workspace/edm_yocto/downloads/imx-codec-4.1.6.bin' has md5 checksum 9b4cf958d86941ee35eab9ff90acb2e5 when 041adb904c50f1cee681b7f6d948e853 was expected
File: '/home/user/workspace/edm_yocto/downloads/imx-codec-4.1.6.bin' has sha256 checksum 218cc540fd512a56bbf8dd03deb408614f5416f94cc72a19edd2fc5b8673388a when 1ed94a01fb47b50ec488dc8dfe96e874ae8270af5e1161f693a8bbe09e507abf was expected
If this change is expected (e.g. you have upgraded to a new version without updating the checksums) then you can use these lines within the recipe:
SRC_URI[md5sum] = "9b4cf958d86941ee35eab9ff90acb2e5"
SRC_URI[sha256sum] = "218cc540fd512a56bbf8dd03deb408614f5416f94cc72a19edd2fc5b8673388a"
Otherwise you should retry the download and/or check with upstream to determine if the file has become corrupted or otherwise unexpectedly modified.

ERROR: imx-codec-4.1.6-r0 do_fetch: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-codec-4.1.6.bin;fsl-eula=true'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/user/workspace/edm_yocto/picoimx7/tmp/work/cortexa7hf-neon-mx7d-poky-linux-gnueabi/imx-codec/4.1.6-r0/temp/log.do_fetch.128019
ERROR: Task 2353 (/home/user/workspace/edm_yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/imx-codec/imx-codec_4.1.6.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2090 tasks of which 984 didn't need to be rerun and 1 failed.
No currently running tasks (2090 of 5183)

Summary: 1 task failed:
/home/user/workspace/edm_yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/imx-codec/imx-codec_4.1.6.bb, do_fetch
Summary: There were 9 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

 

It seems "do_fetch failed", I checkde network and tried many times, which were same error.

I don't know how to solve this problem?

thanks

Jackson Williams

Attachments

    Outcomes