S32DS for Vision - list of Videos

Document created by Mike Doidge Employee on Sep 18, 2017Last modified by Mike Doidge Employee on May 6, 2019
Version 13Show Document
  • View in full screen mode

Create From Example

1 | Create an ISP Project from Example

A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio.

 

2 | Create an APEX2 Project from Example

A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio.

 

https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS

 

 

Create New Project

3 | Create a New ISP Project

A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio.

 

4 | Create a New APEX2 Project

A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio.

 

https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS

 

 

Debug

 

5 | ISP Debugging w/ S32 Debug Probe

A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe.

 

6 | APEX2 Debugging w/ S32 Debug Probe

A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe.


7 | APEX2 Debugging with Emulator

A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio.

 

8 | Debug a bare-board APEX2 Project

A demonstration of how to debug a bareboard APEX2 image processing application project in the S32 Design Studio with Lauterbach TRACE32.

 

9 | Debug a Linux A53 Project

A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code.

 

10 | Debug a bare-board A53 Project

A demonstration of how to debug a bareboard A53 image processing application project in the S32 Design Studio for Vision version 2.0 using PEMicro GDB interface. The example shown also includes code for APEX, but currently PEMicro only supports debug of the A53 code.

Attachments

    Outcomes