A Patch For FlexCAN RX FIFO ID table structure

Document created by Kan_Li Employee on Nov 15, 2016Last modified by Diana Torres on Feb 28, 2017
Version 2Show Document
  • View in full screen mode

There was a macro definition issue in the flexcan driver of ksdk 2.0, the macros of RX_FIFO_STD_MASK_TYPE_B/C were defined based on maco FLEXCAN_ID_STD(id), for example:

#define FLEXCAN_RX_FIFO_STD_MASK_TYPE_B_HIGH(id, rtr, ide) \
(((uint32_t)((uint32_t)(rtr) << 31) | (uint32_t)((uint32_t)(ide) << 30)) | \
(FLEXCAN_ID_STD(id) << 16)) /**< Standard Rx FIFO Mask helper macro Type B upper part helper macro. */

but FLEXCAN_ID_STD(id) is defined for flexCAN Message Buffer structure, so FLEXCAN_ID_STD(id)  is a value of "id" left-shifted by 18,  according to the spec.

while for RX FIFO ID table structure, the spec of Type B/C is different.

so we should use the value of id directly to define the type B and type C Rx Frame Identifier. For example,

#define FLEXCAN_RX_FIFO_STD_MASK_TYPE_B_HIGH(id, rtr, ide) \
(((uint32_t)((uint32_t)(rtr) << 31) | (uint32_t)((uint32_t)(ide) << 30)) | \
((id & 0x7FF) << 19)) /**< Standard Rx FIFO Mask helper macro Type B upper part helper macro. */

 

This patch doesn't affect FlexCAN operation related with message buffers , neither with RX FIFO A type ID table.

 

Please kindly refer to the attachment for details.

 

Sorry for the inconvenience that has caused.

 

-Kan

4 people found this helpful

Attachments

Outcomes