Protection and Hardware changes_updated.pdf

File uploaded by Philip Drake Employee on Oct 27, 2016Last modified by Diana Torres on Jun 6, 2019
Version 5Show Document
  • View in full screen mode

#Introduction:

This document steps the changing of the TWR-MC-LV3PH board to work at 48V 16 A and how to effect these changes in the KMS tool.

As you begin to customize your hardware this document can be used to supplement the information you need to get your custom board up and running with KMS. Please Add these steps to change the max voltage and/or current values in the KMS tool. 

 

Version 3: Corrected VBUS maximum voltage showing relationship the KMS GUI invokes on the Nominal Motor Bus voltage. 

Version 4: Added paragraph on the sizing of the shunt resistors in response to Pavel's notes.

Regards,

Philip

Outcomes