Building Kinetis example from command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building Kinetis example from command line

Building Kinetis example from command line

This tutorial describes how to build a project from command-line, using the GCC build tools included in the Kinetis Design Studio (KDS) tool from NXP.  KDS uses open-source components including the Eclipse IDE and GCC build tools.  The Eclipse IDE can be configured to automatically create make files for the project.  After KDS creates these make files, they can be used to build the project from the command-line, without using the KDS IDE. 

This tutorial uses an example for the Kinetis KE04Z microcontroller (MCU), using the FRDM-KE04Z development board.  The following software is used in these tutorial steps:

Labels (1)
Attachments
No ratings
Version history
Last update:
‎09-29-2016 10:17 AM
Updated by: