i.MX6 Streaming Media Demo

Document created by Michel Abitteboul Employee on Aug 24, 2016Last modified by Diana Torres on Apr 18, 2017
Version 7Show Document
  • View in full screen mode

This shows an i.MX6 Quad rev 1 -based Streaming audio/video demo which shows how video can be distributed from the central (IVI) system in the car to any connected device such as an Android tablet or an iPad. Video can be played from a local SD card and broadcasted to the connected device in a fully synchronised way. This can be controlled from any device connected to the system and showing the video. This is achieved by running the Cinemo Multimedia Framework on top of the INTEGRITY RTOS.

 

Value Propositions

* Enables the streaming of video and audio to multiple connected devices in the car, e.g. Rear Seat

* All devices are fully synchronised and can control playback

* Takes advantage of the hardware-accelerated video decoder (VPU) of the i.MX6

 

NXP Content: i.MX6 Quad

Attachments

    Outcomes