KL25Z and Sensor Fusion

File uploaded by Mike Stanley Employee on Aug 26, 2016Last modified by Diana Torres on Feb 28, 2017
Version 2Show Document
  • View in full screen mode


The attached was put together in response to the posting by Andrew Hartnett.  It contains a bare-metal IAR project for 9-axis sensor fusion V7.00 on the KL25Z.  You need to have built KSDK for the KL25Z to include the ISSDK option.  Then unzip this file into your SDK_2.0_FRDM-KL25Z/boards directory.  The sample project is then located at SDK_2.0_FRDM-KL25Z/boards/frdmkl25z_virtual_shield/issdk_examples/algorithms/sensorfusion/baremetal_sensor_fusion/iar.

There is also an included freertos_sensor_fusion project.  Ignore that for now.  It compiles and links, but needs more RAM than the KL25Z supplies.  I'm looking at ways to decrease the RAM requirements to fit.