New CodeWarrior for MCU V10.7 is available

Document created by Erich Styger Employee on Aug 4, 2016Last modified by Diana Torres on Feb 28, 2017
Version 3Show Document
  • View in full screen mode


CodeWarrior for MCU V10.7 is now available for download from at
CodeWarrior for Microcontrollers-Eclipse IDE|NXP


Major features

  • Combines all the previous CodeWarrior for MCU V10.6.x downloads into a single download and installer
  • Windows 8 and 10 support
  • Added S12Z and S08 device support
  • Updated P&E and Segger debug libraries
  • Various enhancements and bug fixes

See attached release notes for details.


It is available as 'offline' and 'online' version:

The offline package contains all architectures supported (ColdFire, ColdFire+, S08, RS08, S12, S12/XGATE, S12Z, DSC, Qorivva, Kinetis), while the online setup executuble contains the common parts, and the selected architectures are downloaded on demand.

The setup will install a 30 day temporary professional license which afterwards default to 'special' edition (code size limited) mode. CodeWarrior for MCU V10.7 is compatible with V10.6 and any existing professional V10.6 license can be used with V10.7. It is not necessary to uinstall any previous CodeWarrior version, as V10.7 can be installed side by side with existing CodeArrior versions.



NXP CodeWarrior Team

3 people found this helpful