DES-N1855 High-Speed SERDES Modeling for the PCB and System Environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DES-N1855 High-Speed SERDES Modeling for the PCB and System Environment

DES-N1855 High-Speed SERDES Modeling for the PCB and System Environment

Networking devices use high-speed differential signaling that can exceed 10 Gbps. Circuit design for the transmitter (TX) and receiver (RX) elements in the high speed channel have capabilities of offset signal losses in the PCB and system. This session will review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses. It will also show key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively. This session will also address maximum length of the PCB channel, PCB-specific structures that need to be optimized and the usage of the IBIS-AMI models for 5-10 Gbps operation. Examples of channels from PCB designs at NXP will also be included.

Labels (1)
Attachments
No ratings
Version history
Last update:
‎05-25-2016 02:39 PM
Updated by: