HMB-N1900 Hands-On Workshop: Use NFC Pairing to Connect Multiple Bluetooth® and Wi-Fi® Devices with a Simple Tap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HMB-N1900 Hands-On Workshop: Use NFC Pairing to Connect Multiple Bluetooth® and Wi-Fi® Devices with a Simple Tap

HMB-N1900 Hands-On Workshop: Use NFC Pairing to Connect Multiple Bluetooth® and Wi-Fi® Devices with a Simple Tap

NFC pairing makes life in a multi-device world more convenient. Tap-to-pair has become a common habit when connecting an NFC-enabled smartphone conveniently to a wireless speaker. Bringing this experience to the next level, even a multi-speaker audio system can be set up with NFC. If all speakers are equipped with an NFC chip, you simply tap one speaker to another to establish the Bluetooth® connection. That's what we call a true wireless stereo system - and it works with any phone, no matter if it is NFC-enabled. Same use case can be shown with NFC headsets. The workshop will guide participants through the implementation of an NFC, Bluetooth and Wi-Fi pairing use case. All participants should bring an NFC Enabled Android Device running Android version (Kit Kat) 4.4x or higher. In addition please install "NFC TagWriter" and "NFC TagInfo" from the Google Play Store.

Labels (1)
Attachments
No ratings
Version history
Last update:
‎05-25-2016 09:30 AM
Updated by: