Demo
This demonstration provides an overview of developing with the various components of the LPCXpresso Ecosystem, showing the main features of the LPCXpresso IDE tools, from project import/creation to multi-core debug, trace and power measurement. A variety of LPCXpresso development boards with their built in LPC-Link2 debug probes will be shown off in conjunction with the LPCXpresso IDE. The LPCOpen peripheral drivers and examples will be used, demonstrating features of several of NXP's low power and flexible LPC MCU families
For more information :
LPCXpresso IDE
LPCXpresso Boards
LPC Low Power 32-bit Microcontrollers
Video Link
Hello.
Left and Right balance of the audio of the video in the community page below is offset, which causes dizziness.
There are several others with the same symptom.
(I will attach ones that I had identified)
Would it be possible to fix it?
Best Regards,
Hiroshi Noma 野間 比呂志
Senior Engineer
Security & Connectivity
Application Engineering Department
Customer Application Engineering Division
NXP Semiconductors Japan Ltd
Yebisu Garden Place Tower 24F
4-20-3 Ebisu, Shibuya-ku, Tokyo 150-6024 JAPAN
TEL: +81-3-6732-7867, FAX: +81-3-6732-7947
E-mail: hiroshi.noma@nxp.com<mailto:keiko.irie@nxp.com> URL: www.nxp.com<http://www.nxp.com/>