Voice over Bluetooth® LE (VoBLE)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voice over Bluetooth® LE (VoBLE)

Voice over Bluetooth® LE (VoBLE)

Demo
The demo session focuses on demonstrating the transport of human voice over the Bluetooth Smart protocol on Kinetis Wireless platforms running the Kinetis Bluetooth Low Energy stack. The intended setup is made up of two Kinetis Wireless KW41Z evaluation boards connected to an audio codec board with a headset (headphones + microphone) connected at each end. The audience can use the headsets for a full duplex voice communication experience. This demo session is aimed at showcasing the performance of the Kinetis KW41Z platform

Demo Features

Full duplex voice samples transport over Bluetooth LE transport using Kinetis KW41Z enabled with the Kinetis BLE v4.2 stack

SGTL5000 audio codec for sample processing and Kinetis K24F for used for compression

Interactive component through a pair of headsets for demonstrating the full duplex voice capabilities

NXP Recommends

ProductLink
Kinetis® KW41Z-2.4 GHz Dual Mode: Bluetooth® Low Energy and 802.15.4 Wireless Radio Microcontroller (MCU) based on Arm® Cortex®-M0+ Corehttps://www.nxp.com/products/wireless/thread/kinetis-kw41z-2.4-ghz-dual-mode-bluetooth-low-energy-an...
Ultra-Low-Power Audio Codechttps://www.nxp.com/products/audio/audio-converters/ultra-low-power-audio-codec:SGTL5000?&fsrch=1&sr...
Kinetis® K24 120 MHz MCU Tower® System ModuleTWR-K24F120M|Tower System Board|Kinetis® MCUs | NXP 

149026_149026.pngpastedImage_0.png

Labels (1)
Tags (2)
Comments

Hello Sir,

     Thanks for VoBLE demo. My customer, Pagatron is interested in this VoBLE application. Could you share more information and materials how to setup it ? My customer is surveying the possibility of using KW35/36 to develop VoBLE.

No ratings
Version history
Last update:
‎05-09-2016 11:51 AM
Updated by:
NXP Employee