Datapath Software Acceleration using DPAA 2.0

Document created by Diana Torres Employee on May 6, 2016Last modified by Diana Torres Employee on Apr 18, 2017
Version 9Show Document
  • View in full screen mode

This demo shows AIOP based data path offload for some of the popular Network Functions: IP Forward, IPSec, Netflow and Open Flow

 

 

 

 

Features:

  • The Data path offload software is 'C' program running in the AIOP and provides control interface at the GPP for integrating with the GPP based control stack.
  • The demonstration shows functionality of the above mentioned popular network applications live in the pedestal.
  • Performance demonstration of the above mentioned popular network applications using remote setup.
  • This implementation uses AIOP hardware accelerators – Table Lookup Unit, Statistics Engine,Timer Manager, Security Engine, Parser, CDMA/FDMA.

 

_______________________________________________________________________________________________________

 

Featured NXP Products:

_______________________________________________________________________________________________________

 

 

N09

Attachments

    Outcomes