RGB TFT Interface Using FlexIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGB TFT Interface Using FlexIO

RGB TFT Interface Using FlexIO

Demo

This demo shows how the FlexIO peripheral can be utilized to connect directly to an RGB TFT display to deliver a rich graphical display. The demo uses the versatile Tower ecosystem to connect the TWR-K80F150M MCU board to the display. The demo is well documented by an Application note and associated software.

 

 

 

Features:

  • Dynamic Graphical LCD (480x272) with 16bt RGB interface
  • Images stored in fast external Serial NOR flash          
  • FlexIO utilized to generate 16bit interface to TFT display with minimal CPU intervention

 

_______________________________________________________________________________________________________

 

 

Featured NXP Products

ProductLink
Kinetis® K8x Secure Microcontrollers (MCUs) based on Arm® Cortex®-M4 Corehttps://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...
Tower® System Modular Development Board Platformhttps://www.nxp.com/design/development-boards/tower-development-boards:TOWER_HOME?&tid=vantower
Kinetis® K80 MCU Tower® System ModuleTWR-K80F150M|Tower® System Board|Kinetis® MCUs | NXP 

 

Application Notes

_______________________________________________________________________________________________________

 

 

 

148734_148734.pngpastedImage_23.png

Labels (1)
No ratings
Version history
Last update:
‎05-05-2016 04:55 PM
Updated by: