The Embedded Artists LPC3250 based board ships with the kickstart loader and Stage 1 Loader (S1L) pre-installed to execute from large block NAND FLASH. The kickstart loader resides in NAND block 0 and is loaded into IRAM with the LPC32x0 boot ROM on chip reset. Control is then transferred to IRAM after the kickstart loader is loaded. The kickstart loader then loads S1L from block 1 and on of NAND FLASH into IRAM. Once S1L is loaded, control is transferred to S1L.