This example implements a mass storage class host mode device that enumerates a mass storage class device (USB flash drive). It reads the first sector of the device and displays a hexdump style listing of that data on a terminal.
The software that makes up this example is designed to run on many different development boards. Therefore the compiler must be configured to build an image that is targeted to the development board you are using. This section explains how to set these build configurations for each of the supported compilers.
Configure projects
right click on the BSP project in the project explorer window
click Build Configurations->Set Active->(see configuration in table below)
repeat these steps with the CDL, nxpUSBlib, and Example_MassStorageHost
Configure MCU
right click on the Example_MassStorageHost project in the project explorer window
click Properties->C/C++ Build->MCU settings->(see configuration in table below)
Configure the indexer
click Window->Preferences->C/C++->Indexer->Use active build configuration
BSP | CDL | nxpUSBlib | Example_MassStorageDevice | MCU | |
LPC1850 / Hitex | LPC18xx_HITEX | LPC18xx | LPC18xx_Host | LPC18xx | LPC1850 |
LPC4330 / Xplorer | LPC4330_Xplorer | LPC18xx | LPC18xx_Host | LPC18xx | LPC4330 |
LPC4350 / Element14 | LPC1435_ELEMENT14 | LPC18xx | LPC18xx_Host | LPC18xx | LPC4350 |
LPC1768 / MCB1700 | LPC1768_MCB1700 | LPC17xx | LPC17xx_Host | LPC17xx | LPC1768 |
LPC1768 / LPCXpresso | LPC17xx_LPCXpressoRevB | LPC17xx | LPC17xx_Host | LPC17xx | LPC1768 |
NOTE: The LPC18xx CDL is used with boards that hold LPC43xx parts. This is done because the LPC43xx CDL is currently experimental. The LPC18xx USB library is used because both parts share the same controller.
Configure a Batch Build
click on Project->Batch Build...
expand the BSP project to display a list of project targets
select the project target by checking the appropriate checkbox (see target list in table below)
repeat these steps with the CDL, nxpUSBlib_Host, and Example_MassStorageDevice
BSP | CDL | nxpUSBlib_Host | Example_MassStorageDevice | |
LPC1850 / Hitex | HITEX1800 | LPC18xx | LPC18xx_Host | HITEX1800 |
LPC1768 / MCB1700 | MCB1700 | LPC17xx | LPC17xx_Host | MCB1700 |
schematic ./BSP/schematics/HITEX_SCM_LPC1850EVA-A2-2.pdf
Connect the JTAG to the 20 pin receptacle marked X4 JTAG
Connect a USB flash drive into the type A receptacle marked X10
Connect a 9-pin serial cable into the receptacle marked UART X1. Connect the other end of this cable into a PC running a terminal program.
To power the board:
Connect the type-B end of a powered USB cable into the receptacle marked X13
or
Supply 5v to the DC connector labeled X14
schematic ./BSP/schematics/HITEX_Final_LPC1850EVA-A3.pdf
schematic: ./BSP/schematics/mcb1700-schematics.pdf
Jumper | Setting |
E/U | 1-2 |
UMODE | 1-2 |
D- | Host |
D+ | Host |
VBUS | 1-2 |
VDDIO | 1-2 |
VDDREG | 1-2 |
ISP | removed |
Connect the JTAG debugger to the 20 pin JTAG or 10 pin Cortex Debug connector
Connect a 9 pin serial cable between COM0 on the board and a PC running a terminal program. Baud rate = 9600
Plug a USB flash drive into the type A receptacle marked HOST
To power the board:
Connect the type-B end of a powered USB cable to the type-B receptacle labeled 'Device'
or
Supply 5v to the -VIN+ pins between the JTAG and COM0 receptacles
Once the board is powered the following LEDs should be illuminated:
Power
100MHz
USC
schematic: ./BSP/schematics/LPCXpressoLPC1769revB.pdf
Plug the LPCXpresso LPC1769 board into the connector labeled J4 on a
LPCXpresso base board
Connect the JTAG to the mini USB receptacle labeled J3 on the LPCXpresso LPC1769
board
Configure the base board according to the users guide from Embedded Artists
Install jumpers 1-2, 3-4, 5-6 on the jumper block marked J61 on the base board
Plug a USB flash drive into the type A receptacle marked J60 on the base board
Connect the mini type-B end of a USB cable to the USB-to-serial receptacle on
the base board labeled X3 and the type-A end to the USB receptacle on a PC.
Once the USB cable is connected to the board the following LEDs should be
illuminated:
LED25 (vbus)
LED26 (3.3v rail)
Use a PC running Windows XP, Vista or 7 to display runtime diagnostics that can be viewed with a terminal emulation program like Teraterm or Hyperterm. The baud rate in these programs should be set to 9600.
In the project explorer window of the IDE right click on the Example_MassStorageHost project and select Debug As->C/C++ MCU Application
In the main window of the IDE click Run->Resume to start running the application
In the Batch Build window, select the project targets as described in Compiler Build Configurations and then click Build
In the main window of the IDE click Debug->Start/Stop Debug Session click Debug->Run
When the example is first run the terminal window will display:
Mass Storage Host Demo running.
When a flash drive is plugged in the terminal window will display
something similar to this:
Device Attached.
Total LUNs: 1 - Using first LUN in device.
Vendor "USB ", Product "Flash Disk "
Mass Storage Device Enumerated.
Waiting until ready...
Retrieving Capacity...
1957887 blocks of 512 bytes.
Contents of first block:
33 C0 8E D0 BC 00 7C FB 50 07 50 1F FC BE 1B 7C 3.....|.P.P....|
BF 1B 06 50 57 B9 E5 01 F3 A4 CB BD BE 07 B1 04 ...PW...........
38 6E 00 7C 09 75 13 83 C5 10 E2 F4 CD 18 8B F5 8n.|.u..........
83 C6 10 49 74 19 38 2C 74 F6 A0 B5 07 B4 07 8B ...It.8,t.......
F0 AC 3C 00 74 FC BB 07 00 B4 0E CD 10 EB F2 88 ..<.t...........
4E 10 E8 46 00 73 2A FE 46 10 80 7E 04 0B 74 0B N..F.s*.F..~..t.
80 7E 04 0C 74 05 A0 B6 07 75 D2 80 46 02 06 83 .~..t....u..F...
46 08 06 83 56 0A 00 E8 21 00 73 05 A0 B6 07 EB F...V...!.s.....
BC 81 3E FE 7D 55 AA 74 0B 80 7E 10 00 74 C8 A0 ..>.}U.t..~..t..
B7 07 EB A9 8B FC 1E 57 8B F5 CB BF 05 00 8A 56 .......W.......V
00 B4 08 CD 13 72 23 8A C1 24 3F 98 8A DE 8A FC .....r#..$?.....
43 F7 E3 8B D1 86 D6 B1 06 D2 EE 42 F7 E2 39 56 C..........B..9V
0A 77 23 72 05 39 46 08 73 1C B8 01 02 BB 00 7C .w#r.9F.s......|
8B 4E 02 8B 56 00 CD 13 73 51 4F 74 4E 32 E4 8A .N..V...sQOtN2..
56 00 CD 13 EB E4 8A 56 00 60 BB AA 55 B4 41 CD V......V.`..U.A.
13 72 36 81 FB 55 AA 75 30 F6 C1 01 74 2B 61 60 .r6..U.u0...t+a`
6A 00 6A 00 FF 76 0A FF 76 08 6A 00 68 00 7C 6A j.j..v..v.j.h.|j
01 6A 10 B4 42 8B F4 CD 13 61 61 73 0E 4F 74 0B .j..B....aas.Ot.
32 E4 8A 56 00 CD 13 EB D6 61 F9 C3 49 6E 76 61 2..V.....a..Inva
6C 69 64 20 70 61 72 74 69 74 69 6F 6E 20 74 61 lid partition ta
62 6C 65 00 45 72 72 6F 72 20 6C 6F 61 64 69 6E ble.Error loadin
67 20 6F 70 65 72 61 74 69 6E 67 20 73 79 73 74 g operating syst
65 6D 00 4D 69 73 73 69 6E 67 20 6F 70 65 72 61 em.Missing opera
74 69 6E 67 20 73 79 73 74 65 6D 00 00 00 00 00 ting system.....
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 2C 44 63 18 2E 07 C3 00 00 80 01 .....,Dc........
01 00 06 20 00 77 00 02 00 00 00 DE 1D 00 00 00 ... .w..........
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
00 00 00 00 00 00 00 00 00 00 00 00 00 00 55 AA ..............U.
When the flash drive is unplugged the ternimal window will display:
Device Unattached.