Example MPC5748G PretendedNetworkingCAN S32DS_1.0

File uploaded by Martin Kovar Employee on Mar 24, 2016Last modified by Martin Kovar Employee on Apr 9, 2019
Version 6Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed

* frequency

*

*

* Mode transition to LPU_STOP is executed. CAN_0 is configured to wake up from

*  LPU_STOP to LPU_RUN using message with standard IDE = 0 as a wake up

*  preselected matching criteria. After wake up from LPU_STOP, user

*  LED1 is blinking.

 

*

* Modified files: mem.ld, sections.ld, startup.s, added file z2_restart.s

*

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5748G-324DS, MPC574xG Motherboard

* MCU:             PPC5748GMMN6A 1N81M

* Fsys:            PLL0 160MHz

* Debugger:        Lauterbach Trace32

*                  PeMicro USB-ML-PPCNEXUS

* Target:          internal_FLASH (debug mode, release mode)

* EVB connection:  Default

*

*

*

********************************************************************************

Outcomes