Stereo Camera using i.MX6 IPU

Document created by Iain Galloway Employee on Nov 6, 2015Last modified by edk on Apr 18, 2017
Version 5Show Document
  • View in full screen mode

Stereo camera using 2 Aptina CMOS sensors connected to an i.MX6 Dual module.

Each stream is managed by a IPUs (Image Processor Unit). The two streams can be encoded and streamed out through the Ethernet interface.

The stereo camera board needs to be connected to a carrier board.

 

Value Propositions

* High performance

* Demonstrate the parallel use of the two IPUs

* Low-cost-module

Attachments

    Outcomes