Long Range Keyless Entry

Document created by Lauren Percy Employee on Oct 26, 2015Last modified by Adrian Puga Candelario on Aug 2, 2019
Version 9Show Document
  • View in full screen mode

This demo shows the maximum range of a typical fob as a function of “gain mode” and “driver current”.

328847.PNG

Value Propositions

* The combination offers a maximum LF distance for convenience functions such as welcome light, walk-away locking or distance bonding

* Achieving more LF distance depends on two factors: receive sensitivity on the key side as well as transmit power at the car side: both effects can be displayed with this demo up to 9 different setup scenarios can be displayed

* 3 best in class gain/sensitivity modes on the key side offer full freedom of design for any use case

* Maximum distances of up to 10m in LF range can be achieved.

Demonstration of long range key fob control for keyless entry with specialized development platform.

 

FEATURES

  • 10m LF range
  • Distance bonding
  • Walk-away locking functionality
  • Welcome light

RECOMMENDED PRODUCTS

NJJ29C0

Attachments

    Outcomes