Embedded Access Door Counter

Document created by Lauren Percy Employee on Oct 26, 2015Last modified by edk on Jun 13, 2017
Version 6Show Document
  • View in full screen mode

Description: 
This demo gathers visitor count data from the light beam and send it to a cloud server thanks to the IoT Reference Platform. The beam Light, with its Power Supply, is connected to an Arduino Shield featuring a segment LCD. The Arduino Shield is connected to a FRDM-K64F board which is acquiring the counter data and is transmitting them to the TWR-K70 board through an Ethernet connection.

On both K70 Tower and K64 Freedom board is running the MQX RTOS and the associated TCP/IP stack. FRDM board has a static IP address and K70 TWR has a DHCP IP assigned by the router installed on the truck. The FRDM-K64 and Arduino shield are displaying the visitor count on the display as well. In parallel the FRDM-K64 is sending the same data to the Tower board.
The visitor counter can be visualized on the cloud at www.thingspeak.com from any computer or mobile phone.

 

Value Propositions

Create an IoT Application without having to implement the protocols 

Leverage the MQX operating system with TCP/IP

 

NXP Content:

FRDM-K64F, K70 Tower board

Attachments

    Outcomes