Baby Seat Monitor Product

Document created by Lauren Percy Employee on Oct 26, 2015Last modified by Martha Diana Torres Ramirez on Apr 18, 2017
Version 9Show Document
  • View in full screen mode

iremind.pngFeatures a force sensor connected with BLE SOC. As soon as it is occupied it connects to the App on the iPhone, and shows the temperature of the seat as well.

 

"iRemind Child Car Seat Alarm with the WIRELESS option is utilizing a iPhone app for notification and audible alarm, the app can be found in the App Store. The iPhone app will beep when the child is placed in the car seat notifying the user the system is activated. The iPhone app triggers an audible alarm on the phone when the phone is a distance of 15′ or greater away from the sensor pad. Battery life of 12 months with normal usage."

 

FEATURES

Hardware Specifications

  • Bluetooth low energy

 

RECOMMENDED PRODUCTS

ProductDescription
QN902xBluetooth Low Energy SoC

RESOURCES

Attachments

    Outcomes