Now Available: MQX RTOS for Kinetis SDK v1.3.0

Document created by Ackey Cheng Employee on Oct 19, 2015Last modified by Diana Torres on Jan 11, 2018
Version 2Show Document
  • View in full screen mode

We are pleased to announce the release of MQX RTOS for Kinetis SDK v1.3.

 

Boards Supported

FRDM-K22F

FRDM-K64F

FRDM-KL46Z

FRDM-KW24

FRDM-KL43Z

FRDM-KL27Z

FRDM-KL25Z

FRDM-KL26Z

USB-KW24D512

MRB-KW01

TWR-K22F120M

TWR-KV31F120M

TWR-K24F120M

TWR-K64F120M

TWR-KV10Z32

TWR-K60D100M

TWR-KL46Z

TWR-K21D50M

TWR-K21F120M

TWR-KW24D512

TWR-KL43Z48M

TWR-K65F180M

 

New Features and Updates

  • MQX RTOS - version 5.0.3 Updates
    • MQX RTOS Kernel has been updated to address several issues related to the task restart and the timer component
  • RTCS - version 4.2.0 Updates
    • The CyaSSL 3.3.0 was upgraded to the WolfSSL version 3.4.6. The location of the library was changed from the middleware/tcpip/rtcs/source/ssl to the middleware/security/wolfssl. The library usage is demonstrated in the
      middleware/tcpip/rtcs/examples/httpsrv example application.
  • Other Updates
    • Added two example applications demonstrating the Kinetis cryptography capabilities - WolfSSL crypto library benchmark : \examples\<board>\demo_apps\security\benchmark_wolfssl

 

How to Get Started

Note: As of Kinetis SDK v1.2, MQX RTOS components are available in the Kinetis SDK itself.

 

1. Visit http://www.freescale.com/ksdk

 

2. Click Download

2015-05-11 16_07_38-Freescale MQX™ Software Solutions_Freescale.png

3. Click KSDK v1.3.0 Mainline Release

4. Review and click to agree to the license terms if they are acceptable.

 

5. Click and installer for your Host OS.

 

6. Download and Install.

 

On Windows, the default source installation directory is C:\Freescale\KSDK_1.3.0

 

7. Check out the getting started guides in the /docs directory.

 

Enjoy!  Best of luck with your embedded projects!

Attachments

    Outcomes