There are several vulnerabilities been found recently as below:
They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.
All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.
To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.
Reference:
https://github.com/WhisperSystems/TextSecure/issues/381
This document was generated from the following discussion: Android vulnerability related with stagefright
Created by Hui Fang