P5020/P5010 COP/JTAG Specific FAQs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020/P5010 COP/JTAG Specific FAQs

P5020/P5010 COP/JTAG Specific FAQs

The JTAG IDCODE for P5010 is 0x0020c01d. What's the IDCODE for the P5010?

Below are the JTAG IDCODES for P5010 and P5020:

P5010: 0x0020_D_01D

P5020: 0x0020_C_01D

For P5020, COP header has COP_CHKSTP_OUT and COP_CHKSTP_IN connections. Are they actually driven by the run control device (USB TAP)? If I leave the pins appropriately terminated then I do not need to route them to an adapter cable, right?

The USBtap does not use these signals at all. It's okay to leave these pins on the cop header as a NC. You do not need to route them to an adapter cable.


For P5020, VDD_SENSE on COP header uses 10-Ohm to OVDD while VIO VSense on Aurora header uses 1K pull-up to OVDD. If I use the 1K Ohm then it will be okay for the USB TAP, right?

Yes, this is okay for the USB TAP. They definitely use the VDD_SENSE pin, but they draw very little current, so there's almost no voltage drop.


COP header has a COP_SRESET# connection on pin #11 which connects to HRESET# on the P5020. The Aurora header does not have this connection. Is it actually necessary for COP header to drive HRESET# on the P5020 device?

The USB TAP does not use the /SRESET pin on the COP header at all. You don't need to route this to the COP header also. You can leave it NC.



Labels (1)
No ratings
Version history
Last update:
‎08-06-2012 11:39 AM
Updated by: