Download And Install Codewarrior 2.8

Document created by GUO XIAOLI Employee on Jul 17, 2012
Version 1Show Document
  • View in full screen mode

1. Download CodeWarrior 2.8 Evaluation Version (Classic, Windows-hosted)

 

To Program your microcontroller you will need to set up the CodeWarrior Integrated Development Environment. CodeWarrior is available on the Freescale.com Website.

 

Method 1: Direct Link
direct download link (Caution - link may not be up to date)

 

Method 2: Navigate to the Download Link

 

From Freescale.com click on:

  1. "Design Resources" tab at the top of the page,
  2. then navigate to "Software and Tools",
  3. and then to "Codewarrior Devleopment Tools"
  4. Click on the "Download CodeWarrior now link"
  5. Click on the Download Evaluation Versions link"
  6. Within this page, use your browser "find" feature (Typically CTRL-F) to search for the text string "V2.8"
  7. Click the "download" button next to "Evaluation: CodeWarrior for MPC55xx/MPC56xx Microcontrollers V2.8 (Classic)". and save it to your computer.

2. Install CodeWarrior

 

To install CodeWarrior Development Studio for Microcontrollers v2.8, double-click the installation
package and a wizard will guide you through the installation process.

Installation Notes:

 

Are you using Windows Vista or Windows 7?

 

Evaluation Edition User:

If you are installing the Evaluation Edition, the Evaluation license is automatically installed with your
product and you do not need to register it. This license allows you to develop projects as
Professional Edition within the 30-day evaluation period. After 30 days, the license works as Special
Edition license (free permanent, but feature limited) which supports unlimited assembly code, up to
32KB of C code for HCS08/RS08 derivatives, up to 64KB of C code for V1 ColdFire derivatives and
up to 128KB of C code for V2-V4 ColdFire and Kinetis derivatives and up to 512KB of C code for
MPC56xx derivatives.

 

Once you have finished downloading and installing CodeWarrior, users can return to Downloading and Installing P&E as part of the Blink a LED on Qorivva Tutorial

 

Attachments

    Outcomes