FTF 2015 Secure Connected Smart Home Definition

Document created by Bill Krakar Employee on Jul 29, 2015Last modified by Diana Torres on Feb 2, 2016
Version 12Show Document
  • View in full screen mode

FTF 2015 Secure Connected Smart Home Overview

  • Multiple heterogeneous IoT wireless and wired networks managed from a single interface
  • Simultaneous support for AllJoyn, WiFi, Thread, HomeKit, ZigBee, etc.
  • Highlights sensors, connectivity, edge devices, and gateways
  • Integrated support demonstrated for multiple partners and production customers

DOC-106605.png

This Demo Is Probably of Interest If You:

  • Need to combine multiple connectivity types into a single managed network
  • Need to support both legacy and state of the art edge devices/connectivity
  • Work with home automation, smart energy or other similar IoT applications

Differentiation This Demo Highlights

  • How to leverage i.MX6 3D graphics rendering for connected smart applications
  • Use of advanced connectivity techniques such as Dual PAN 802.15.4 radios
  • How to manage and control disparate networks from a single location

Description

The FTF 2015 Secure Connected Smart Home was created to highlight our unique ability to field real world IoT capabilities from sensors, to state of the art wireless connectivity, to edge devices, to advanced multi-media connected smart devices acting as primary controllers, gateways, border routers for next generation IoT systems.

The Smart Home combines actual customer product prototypes or beta deliverables along with development platforms to provide a unique experience of what real customers are doing with our technology today, as well as showcasing the silicon, platforms and tools developers can use to create their next generation IoT products.

 

The Smart Home includes:

  • Sensors including the latest version of the Intelligent Sensing Framework (ISF)
  • NXP and partner wireless connectivity
    • 802.15.4
    • ZigBee (ZLL, RF4CE, HA, SE)
    • Thread
    • BLE
    • WiFi
  • Kinetis Edge Devices
  • i.MX Connected Smart Devices/Border Routers/IoT Gateways
  • Advanced UI touch panel with full 3D graphics rendering
  • Integrated IoT network management facility

 

Full Listing of Products/Components

Note: For full listing or additional information for Products/Components used in this demo see "This Demo's IoT Highlights" in Left Column and Additional Products/Components below that. Note: If you aren't looking at this demo in the IoT Center, please use below link to access IoT Center:

FTF 2015 Secure Connected Smart Home

 

FTF Smart Home Videos

Overview of the FTF Smart Home

 

Strong Authentication Front Door

Advanced UI Touch Panel w/ 3D Graphics

 

Home Automation and Audio

 

Thread Overview

Thread Connectivity Demos

Bluetooth Smart

Attachments

    Outcomes