Making of toolchain including Qt5 at i.mx6SoloLite Evaluation Kit

Document created by kazuoasano on Jul 21, 2015
Version 1Show Document
  • View in full screen mode

Hi All


I make fsl-image-qt5 in yocto.

make command:

$ MACHINE=imx6slevk source -b build -e fb

$ bitbake fsl-image-qt5


However, I couldn't make meta-toolchin-qt5 in yocto.

The error is as follows.


> | WARNING: exit code 1 from a shell command.

> | ERROR: Function failed: do_configure (log file is located at /opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtdeclarative/5.3.2-r0/temp/log.do_configure.3411)

> ERROR: Task 771 (/opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/sources/meta-qt5/recipes-qt/qt5/, do_configure) failed with exit code '1'

> NOTE: Tasks Summary: Attempted 1235 tasks of which 1234 didn't need to be rerun and 1 failed.

> No currently running tasks (1234 of 3376)


> Summary: 1 task failed:

>   /opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/sources/meta-qt5/recipes-qt/qt5/, do_configure

> Summary: There was 1 ERROR message shown, returning a non-zero exit code.


How do you make toolchain include Qt5?