Generate random ethernet mac And program it to eFuse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate random ethernet mac And program it to eFuse

Generate random ethernet mac And program it to eFuse

Abstract:

On the time otp driver initializes, it will check the mac bits of eFuse,  when the value is invalid, generate a random mac, and program  it to eFuse.

Environment:

i.mx6dl

android-4.2.2

kernel-3.0.35

Changes:

1. kernel_imx/arch/arm/mach-mx6/mx6_fec.c

----------------------------------------------------------------

void __init imx6_init_fec(struct fec_platform_data fec_data)

{

  fec_get_mac_addr(fec_data.mac);

  if (!is_valid_ether_addr(fec_data.mac))

      fec_data.mac[0] = 0x10; // changed by xxx

  if (cpu_is_mx6sl())

  imx6sl_add_fec(&fec_data);

  else

  imx6q_add_fec(&fec_data);

}

2. kernel_imx/drivers/char/fsl_otp.c

----------------------------------------------------------------

//add by xxx

static void check_otp_mac(void)

{

  unsigned int index_mac0 = 34;

  unsigned int index_mac1 = 35;

  u32 value_mac0 = 0;

  u32 value_mac1 = 0;

  u32 value_random_mac0 = 0;

  u32 value_random_mac1 = 0;

  char otp_mac[6], random_mac[6];

  memset(otp_mac, 0, sizeof(otp_mac));

  memset(random_mac, 0, sizeof(random_mac));

  mutex_lock(&otp_mutex);

  //get

  if (otp_read_prepare(otp_data)) {

  mutex_unlock(&otp_mutex);

  return 0;

  }

  value_mac0 = __raw_readl(REGS_OCOTP_BASE + HW_OCOTP_CUSTn(index_mac0));

  value_mac1 = __raw_readl(REGS_OCOTP_BASE + HW_OCOTP_CUSTn(index_mac1));

  otp_read_post(otp_data);

  mutex_unlock(&otp_mutex);

  if(value_mac0 != 0 && value_mac1 != 0)

  {

  otp_mac[5] = value_mac0 & 0xff;

  otp_mac[4] = (value_mac0 >> 8) & 0xff;

  otp_mac[3] = (value_mac0 >> 16) & 0xff;

  otp_mac[2] = (value_mac0 >> 24) & 0xff;

  otp_mac[1] = value_mac1 & 0xff;

  otp_mac[0] = (value_mac1 >> 8) & 0xff;

  }

  printk("otp_mac=%pM\n", otp_mac);

  //check

  if (!is_valid_ether_addr(otp_mac))

  {

  random_ether_addr(random_mac);

  printk("get random mac:%pM\n", random_mac);

  //set

  value_random_mac0 = 0;

  value_random_mac0 = value_random_mac0 | random_mac[2];

  value_random_mac0 = (value_random_mac0 << 8) | random_mac[3];

  value_random_mac0 = (value_random_mac0 << 8) | random_mac[4];

  value_random_mac0 = (value_random_mac0 << 8) | random_mac[5];

  value_random_mac1 = 0;

  value_random_mac1 = value_random_mac1 | random_mac[0];

  value_random_mac1 = (value_random_mac1 << 8) | random_mac[1];

  mutex_lock(&otp_mutex);

  if (otp_write_prepare(otp_data)) {

  mutex_unlock(&otp_mutex);

  return 0;

  }

  otp_write_bits(index_mac0, value_random_mac0, 0x3e77);

  otp_write_bits(index_mac1, value_random_mac1, 0x3e77);

  otp_write_post(otp_data);

  mutex_unlock(&otp_mutex);

  }

}

//end

3.  kernel_imx/drivers/char/fsl_otp.c

----------------------------------------------------------------

static int __devinit fsl_otp_probe(struct platform_device *pdev)

{

  ...

  retval = sysfs_create_group(otp_kobj, &attr_group);

  if (retval)

  goto error;

  mutex_init(&otp_mutex);

  //add by xxx

  check_otp_mac();

  //end

Tags (2)
No ratings
Version history
Last update:
‎07-07-2015 10:10 PM
Updated by: