FTF-ACC-F1112.pdf

File uploaded by freescaletraining on Jun 19, 2015Last modified by freescaletraining on Sep 24, 2018
Version 2Show Document
  • View in full screen mode

S32 Design Studio for ARM is a hands-on training with the new Eclipse-based tool chain with C development tools in the integrated development environment including editor, compiler, and debugger support of Freescale's latest automotive ARM-based MCUs. Participants will learn about the project creation, editing, compiling, Processor Expert configuration tool, and debugging of a small example project under the direction of one of Freescale's tools experts. The class will focus on the Freescale KEA MCUs with the highly-integrated, easy-to-use tool chain. The student will start with a project from scratch, work through new project creation, configuration of the compiler, compilation, flashing executable onto the target MCU and complete the class with debugging the project on the target MCU evaluation board.

Attachments

Outcomes