Hi All,
I am also facing the same problem, Please help me to get out of this problem.
Platform : IMX6SL
Bluedroid on Android kitkat 4.4.3.
Can you please help me I am struck at this point not able to move forward.
D/BluetoothAdapterState( 704): CURRENT_STATE=PENDING, MESSAGE = ENABLE_TIMEOUT, isTurningOn=true, isTurningOff=false
E/BluetoothAdapterState( 704): Error enabling Bluetooth
D/BluetoothAdapterProperties( 704): Setting state to 10
I/BluetoothAdapterState( 704): Bluetooth adapter state changed: 11-> 10
D/BluetoothAdapterService( 704): Broadcasting updateAdapterState() to 1 receivers.
Hi all,
I am glad to inform you that the above issue which I have posted earlier got resolved, but I have another 2 issues one while data transfer, the other while enabling via GUI.
1) After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :
File not Received
File : sample.jpg
Reason : Storage issue
2) And presently I am inserting my driver via GUI, I am getting an error message while enabling bluetooth via GUI ie Operation not permitted while loading .ko (driver)Please suggest me what to do?? whether I need to install my driver at boot by adding in init.rc?? if I do it always on boot bt will be in ON State only?? OR Do i need to build my driver along with android source code???
Please suggest me how to proceed further???
Thanks and Regards,
Mutyala Rao.
Hi all,
I am able to resolve the above two issues like this.
1. Installed the apk.file using ADB (Android Debugger) by following this link:
https://androidonlinux.wordpress.com/2013/05/12/setting-up-adb-on-linux/
2. I have inserted the modules on boot. by placing the path of the modules in init.freescale.rc located in the path myandroid/out/target/product/evk_6sl/root/
Hi Mutyalarao,
I am facing the same issue with you. Could you tell me how did you solve this issue when turn on wifi?
Very appreciate.
root@sabresd_6dq:/ # D/WifiService( 2727): setWifiEnabled: true pid=3073, uid=1000
W/WifiHW ( 2727):
W/WifiHW ( 2727): ---------------SN=--------->>>>>>>wifi_load
_driver
E/WifiHW ( 2727): +++++type=1400 audit(86590.640:5): avc: denied { module_request } for pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system
+ wifi_load_driver
type=1400 audit(86590.660:6): avc: denied { sys_module } for pid=2681 comm="netd" capability=16 scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability
type=1400 audit(86590.680:7): avc: denied { module_request } for pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system
type=1400 audit(86590.700:8): avc: denied { sys_module } for pid=2681 comm="netd" capability=16 scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability
type=1400 audit(86590.710:9): avc: denied { module_request } for pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system
type=1400 audit(86590.720:10): avc: denied { sys_module } for pid=2681 comm="netd" capability=16 scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability
type=1400 audit(86590.740:11): avc: denied { module_request } for pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system
type=1400 audit(86590.760:12): avc: denied { sys_module } for pid=2681 comm="netd" capability=16 scontext=u:r:netd:s0 tcontext=u:r:netd:s0 tclass=capability
type=1400 audit(86590.780:13): avc: denied { module_request } for pid=2681 comm="netd" kmod="netdev-wlan0" scontext=u:r:netd:s0 tcontext=u:r:kernel:s0 tclass=system
Thanks,
Wayne